Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The
configuration file is automatically copied into the local user directory
as din 962_local.cfg
.
In the following the settings are described:
All settings are made in the [SYSTEM] block.
DISABLE_FEATURE=0/1
DISPLAY_BUTTON=0/1
0: button invisible (possibly grayed; see BUTTON_ENABLED); 1: button visible
Note | |
---|---|
It only makes sense to use the function if DISPLAY_BUTTON=1is also set. The button is only then activated if DIN962 columns in the table are available. |
BUTTON_ENABLED=0/1
0: button deactivated (grayed); 1: the button may be used if DISPLAY_BUTTON=1.
BUTTON_PRESSED=1
The setting can be used optionally.
If BUTTON_PRESSED=1, the user settings are over written. If it is not set, the user settings of the din962_user.cfg configuration file are read.