Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Note | |
---|---|
Prerequisite for the installation of Windchill PDMLink is that the CAD interface is installed properly. |
In addition, a connection to the server must be present as well.
Open Tools -> Server registration in ProE.
-> The server registration dialog shows up in which one can select the server and set up the library.
Choose Server -> Register new server.
Under Name enter a name for the server. Under Storage location the IP address of the server is entered. Here it is important to set /Windchill after the server name. Only then will a server be found.
If you click on Check the existing library is searched through. It is then displayed in the lower window. If you are searching for the correct library and then click on OK, the workspace will now use this library as the workspace of the user in ProE.