powered by CADENAS

Manual

Manual

5.9.2.3.2.  Try NT user authentication

Basic requirement for the use of this function is the operation of a MS-SQL or Oracle database. The SAPDB does not enable a NT user authentication, for example.

Advantage: Through the user authentication the manual registration at the LinkDB is omitted. The user does not receive a login window! If the user only has one role, the role selection dialog also gets omitted.

Requirements for the implementation of the function:

  1. In order to engage the NT user authentication, mark the Try NT user authentication checkbox after you have activated the ERP environment in the assortment of the category tree.

  1. Upon configuring the driver, the option with Windows NT authentication by means of user name in the network must be selected.

    Example MSSQL-Server:

    Open configuration window via START --> Settings --> Control Panel --> Administration --> Data sources (ODBC) --> Register System DSN --> Add / Configure --> 2nd settings window

  1. One should pay attention to the fact that the option "The standard database change to" is set and the responsible database is given.

  1. The appropriate user name with the Windows NT authentication option must be applied in the database server.