powered by CADENAS

Manual

Manual

1.1.4.8.  Document types

Allocations of symbols, applications, etc. to Document types

Small symbol / Large symbol: These symbols can be used for the project view. (Acroread etc...)

Application (WIN) / Application (UNIX): File path to program file:

[Note] Note

Do not forget to set "'spaces'%1" as additional parameter behind the directory information! (Placeholder for file)

The DDE commands serve for controlling the external programs under Windows. Under Unix, DDE has no meaning.

Copy symbol files to $CADENAS_SETUP: The symbols applied under Small symbol and Large symbol become generally accessible for PARTsolutions-User.

[Note] Note

The settings dialog for the Document types is also available in the PARTdataManager under Extras -> Settings... -> Part selection. See also Section 3.1.3.3.1.2.22, “ Create document project ” in PARTsolutions / PARTcommunity4Enterprise - User manual.