Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In order to locally apply users in PARTsolutions, do the following:
You have the following options:
Dialog area Database user -> button Create locally
Using this command means that the user displayed in the Database user window is collected in PARTsolutions. The corresponding user then shows up in the User window. He is also taken over into the plinkusers.cfg configuration file.
Note | |
---|---|
This method guarantees that the database user taken over by PARTsolutions truly exists in the database. (Only such are even displayed in the Database user dialog area.) |
Dialog area User-Role assignment -> User -> button New
Note | |
---|---|
The user is now applied in PARTsolutions. If you want to apply users in this method, you must make sure that the respective user actually exists in the database (see Section 5.6.2.2, “ Apply user via PARTadmin ”). |
User-Role assignment dialog area -> User -> Copy button.