Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
1.1.7.5.10. varsearch.cfg
1.1.7.5.10.1. Full text
search: Priority setting of the fields to search
|
|
---|---|
Prev | Next |
The priority of fields to search can
be set under $(CADENAS_USER)/varsearch.cfg
.
Normally the default settings don't have to be adjusted (but can optionally).
If a field shall not be searched, then remove the specific statement from the value range.
If a field shall get a higher prioritization, then set a higher value (1000 for example).
"orderno" is the field for the order number defined in eCAT.
The explicit stating of the path is not possible yet.
[VariableSearch] FieldPriorizations=CNS_SEARCHDATA=1.0,orderno=150.0,nn=100.0,nt=60.0,nb=30.0
The synonym search uses the same settings as above, however with the factor stated here. The default value of 0.3 says that hits, which result form the synonym search have lower priority than direct hits.
SynonymFieldPriorizationMultiplicator=0.30