powered by CADENAS

Manual

Manual

1.1.4.3.4.1. Structure of the dialog and meaning of symbols

The dialog includes 2 tabbed pages:

  • Catalog list:

    All settings are made here.

  • Migration:

    The migrations process is protocolled here. At the end you are informed whether the migration was completed successfully.

Catalog list tabbed page

  • On the top left the individual steps of the migration process are listed.

    • 1. Load catalog list

    • 2. Select tasks

    • 3. Start migration

  • On the bottom left in the Legend, the meaning of the symbols used is explained:

    V9 Catalog

    V8 Catalog

    V8 Catalog migrated

    Geometrical index existing (new V9 index)

    Geometric index exists

    Geometric index convertible

    V8 geometry index available. This can be converted into a V9 index.

    [Note] Note

    This needs relatively little time in comparison to a complete new creation of the geometry index for all catalogs.

    No geometry index available

    There is no V9 index available.

  • Available catalogs

    At the right the available catalogs are displayed. The symbol informs you of the status of a catalog.

    Every single catalog can be activated for migration via the checkbox.

    Multiple selection:

    Furthermore you can select several catalogs at once via the following checkboxes:

    Select all

    Select all V8

    Geometry index from V8 convertible

    This assumes that a geometry index has already been made in V8.

    Geometrical index convertible from V9 (Indices <= V9.07)