powered by CADENAS

Manual

Manual

1.1.7.3.4.  Edit configuration entry

By double-clicking on a selected row, the Edit configuration entry window opens.

Here you can:

  • Define Types of values:

    • Alphanumeric (optional allow user input)

    • Numerical (optional allow user input)

    • Categories assign of ... to

  • Edit Help strings and Examples; both the default entry as well as all translation languages.

    "default" should always be filled out; all other languages may be filled out as desired.

    If the language set within PARTsolutions is available in the help text, it will be shown; if not, the default text is displayed.