Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
With distributed locations it may be useful to replicate the LinkDB. Reasons could be that the transmission time is too long, or the necessity to work independently, and the system availability.
What is to be understood by replication?
Data replication is the copying of information to one or more databases in a manner in which the data is equal in all locations. There are basically two different types of synchronisations: synchronous and asynchronous replications. With synchronous replication, the data comparison occurs nearly without any delay. With asynchronous replication, seconds, minutes and possibly even days may go by. In addition, it is important to know whether all so-called subscribers only have reading rights, or whether they are also able to change data.
The current replication tools from Microsoft and Oracle, as well as other providers, are adjustable to special requests and offer plug & play solutions, which can be used with relative little implementation complexity.
On the Microsoft and Oracle internet pages, you can find detailed information about replication.
Note | |
---|---|
Please also note Section 5.2.1, “Hardware requirements ”. Data throughput per time unit and type of part significantly influence the performance. |