powered by CADENAS

Manual

Manual

1.7.8.2.1. Keys "CATMETRICS_*"

When generating the CIP file of a catalog, in the catalog's filedir.prj the results of the resolve check will be set in the form of following keys (for details see Section 5.8.2.1.15.18, “Reverse search ‒ Resolve check (automatic) ” in eCATALOGsolutions Manual):

  • CATMETRICS_SEARCHABLE_PROJECTS

    Number of projects which should be found (All visible projects and projects with SEARCHINDEX=ON)

  • CATMETRICS_REVERSE_CLASSIFIED

    Number of projects with a classified order number or type code variable

  • CATMETRICS_REVERSE_STATIC

    Number of projects without value ranges

  • CATMETRICS_REVERSE_CONFIG

    Number of projects with manual reverse scripts

  • CATMETRICS_REVERSE_LUCENE

    Number of projects with order numbers and type codes indexed by lucene

  • CATMETRICS_REVERSE_GRAPH

    Number of projects which can be solved via auto reverse search

  • CATMETRICS_REVERSE_FAILED

    Number of projects which can't be found by the reverse search

Background information: In order to create the information which shall be written into the dir.prj, the configuration files resolvecheck.cfg and *.qacheck are evaluated. E.g., the ResolveChecker writes to resolvecheck.cfg for which projects an automatic Reverse Search is possible. For the case that someone changed a project without executing the ResolveChecker the information is read from *.qacheck, where Testmeta is writing to, and for changed projects Testmeta has to be called in any case, because otherwise publication is not possible.