powered by CADENAS

Manual

Manual

1.3.8.4.1.  Generate new display index

Via the Generate new display index command, you can create a new search index.

[Caution] Caution

As soon as you have clicked on the button, a warning message shows up. This means that personal changes, such as for example hiding certain directory tree folders (see also Section 1.3.8.6.2, “Context menu commands in detail ”), are set back through the creation of a new search index and are thus no longer effective.

If you have made personal changes and would like to keep these, use the command Update display index.

Typical use cases for Generate new display index are changed storage locations for the library directories or restructured Drives.

As soon as you have clicked on Generate new display index the progress display shows up at the bottom under Index update.

Index update

Index update

[Note] Note

Compare context menu command Display index -> Update

Compare context menu command Display index -> Add missing directories to the display index

See context menu commands in detail.