Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The role selection may be controlled via a system variable as well. The desired role is the automatically selected during registration process, regardless whether the user is configured as valid for this role, or whether he has more than one role available. (The configuration file plinkusers.cfg is irrelevant)
Note | |
---|---|
If the key has not been set, nothing happens. If the key is set, then nothing happens either. Only once the content is in the environment value, the function will be carried out. |
Update of full-text search index at each LINKDB change:
UPDATESEARCHINDEX= 0/1
In V9.08 the key was used to update the ERP search index once an ERP number had been added. (Locally on the client)
In V10, when adding an ERP number an entry in the LOGTABLE is made. In this way the "Task" on the AppServer updates the ERP search index. Details on this can be found under Section 5.5.6.2.3.1, “Logging of LinkDB changes ”.
That's why the local creation on the client is "off" per default (UPDATESEARCHINDEX=0).