Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
5.12.1.1.1. Without direct linkage to
the ERP system
5.12.1.1.1.1. Manual entry of
ERP number
|
|
---|---|
Prev | Next |
Manual input of ERP number is default setting when using the PLINKDB. When using PLDBDEMO a timestamp number is automatically created by default.[77]
Select a dataset without ERP number in order to create it and to add the dataset to the link database.
Call the dialog box new ident-no. by clicking on the button Add dataset to link database .
(The display of the button is role-dependent. Possibly it is not available for certain roles.)
|
Enter the ERP number (if not automatically created) and select further values in the list fields and confirm by clicking on OK.
-> The link database dataset with the fields ERP number, Material, Active status and Requested status (default) is immediately shown in PARTdataManager.