Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
[Common] stlMaxTriangleCount
When a geometry import has been cancelled, information on this is displayed in the message window. If a too high amount of "triangles" caused the termination, you can define the maximum allowed amount here.
During installation the proxy settings of the Internet Explorer are set.
http_proxy=.... https_proxy=... ftp_proxy=...
Correct settings are precondition for the working of the assistant window, for example.
Further functions such as call up of company websites are also possible.
You can also transfer the subassembly structure to the CAD system
On this in the
configuration file under $CADENAS_SETUP/partsol.cfg
->
Key ExportSubAssemblyStructure
set the
value on "true".
[COMMON] ExportSubAssemblyStructure=true
The feature is available for all CAD interfaces.
The following figure shows an assembly with subassembly in PARTdataManager.
The following two figures show the assembly structure (exemplarily in Solidworks) once with and once without subassembly.