Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Immediately after activation, PARTsolutions checks in all requested parts into VAULT. PARTsolutions cannot check whether this part was then really integrated or later removed from the assembly. This means that all parts that are exported from PARTsolutions but not used, are still checked into VAULT.
With the exception of the higher storage capacity in VAULT there will be no other disadvantages. If the part is later really integrated, this disadvantage is then also forgotten.
Activation must be done in the %CADENAS_SETUP%\ifvault.cfg file.
With the following two steps the interface is activated:
$CADENAS_SETUP/ifacecommon.cfg
"AppBeforeCreate" and "AppAfterCreate" have to be commented in.
[CreationOptions] AppBeforeCreate=GetObject("pdm.callbackCheckinout").AppBeforeCreate AppAfterCreate=GetObject("pdm.callbackCheckinout").AppAfterCreate
ACTIVE_CONDITION has to be set on "true".
[PLM] ACTIVE_CONDITION=true