Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Show or hide the previews of "Animation", "2-D/3-D", "Technical Details" and "PDF".
[PREVIEW] ;Sets if animation preview is available (as of 1.5) HideAnimationPreview=false ;Sets if the information preview (technical details etc.) are available (as of 1.5) HideInformationPreview=false ;Sets if the 23d preview is available (as of 1.6) Hide23dPreview=false ;Sets if PDF preview is available (as of 1.6) HidePdfPreview=false ;Indicates if ActiveX is enabled (as of 1.0) EnableActiveX=true ;Indicates the current used ActiveX viewer version (as of 1.5) ActiveXViewerVersion=1,0,36,0 ;Set if the 2-D image preview is used (instead of a plugin -applet or active x) ;(as of 1.3) HidePreview2-DViewerPlugin=false ;Set if the information image preview is used (instead of a plugin -applet ;or active x) (as of 1.3) HidePreviewInformationViewerPlugin=false ;Indicates a preview generation error message (as of 1.3) HidePreviewGenerationMessages=true ;Sets if the thumbnails are available for the information preview (technical ;details etc.) (as of 1.3) HidePreviewInformationThumbnail=false ;Sets if the thumbnails are available for the 2-D preview (as of 1.3) HidePreview2-DThumbnail=false ;set to true if the reload frame should be reloaded if ReloadPreviewFrameOnFolderSelect=true ;Sets if preview should be shown for deep links (as of 1.8) LoadPreviewForDeepLink=true
Zurück | Nach oben | Weiter |
4.7.11. LOGIN | Zum Anfang | 4.7.13. PARTcommunity Administration |