Each
installation of the PARTsolutions software (new and update
installation) should only occur, when the network is not used
productively (reference appointment), if data needs to be transferred
via the network.
Depending
on server software, restrictions may fall upon other users.
Note
Make sure
no PARTsolutions applications are open during updates.
Note
Environment variables,
Registry entries
Should entries and/or variables from
older installations still be set, these must be removed in order for
the language adjustment to work properly in PARTadmin.
The
language selection concerning the relation between PARTadmin and
PARTsolutions Version 9 has been changed!
Up to
now PARTadmin always wrote on the environment variable
$CADENAS_LANGUAGE.
Now,
with version 9, PARTadmin writes onto $CADENAS_USER/partsolu.cfg.
($CADENAS_LANGUAGE can, if explicitly desired, continue to be
used. The priorities can be taken from the list in the following
point.)
Now due
to the changeover, users without PARTsolutions admin rights (and
operation system admin rights) can make language settings at the
client computer.
The
following lists, in order of priority, components that affect the
language setting: