Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
You have the following options to start the server installation:
Insert the DVD and wait for the start screen to show up.
On the start screen select the desired language and click on Installation (Server).
Should the
start screen not show up automatically, you can open it at the top
file level via start.exe
.
The setup contains the following windows:
Set up new release (See Section 2.2.2.1.6, “Select release directory / Set up new release ”)
Insert the
DVD and begin the installation at the top file level with psol_workstation.exe
.
The setup contains the following windows:
Set up new release (See Section 2.2.2.1.6, “Select release directory / Set up new release ”)