powered by CADENAS

Manual

Manual

2.2.2.1.  Server installation

You have the following options to start the server installation:

  1. Insert the DVD and wait for the start screen to show up.

    On the start screen select the desired language and click on Installation (Server).

    Enter via start screen

    Enter via start screen

    Should the start screen not show up automatically, you can open it at the top file level via start.exe.

    The setup contains the following windows:

  2. Insert the DVD and begin the installation at the top file level with psol_workstation.exe.

    The setup contains the following windows: