Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
If you want to make a cut between 3-D solid and a 2-D sketch which occurs through the Rotation of the 2-D sketch, please do the following:
In the example, the cuboid should completely be penetrated. In order to create a "total stretch" you must only confirm the Angle at 360°. |
-> After confirming with OK both objects are cut. A circular tube is removed from the cuboid. -> In the History another point (feature) shows up: Cut rotation . |
The explanation of the other fields can be found here Section 10.5.1.4.4.1, “ Extrude... ”.