powered by CADENAS

Manual

Manual

10.5.1.2.2.  Insert Fixed plane...

Via the coordinates of the base point as well as both vectors (x-axis, y-axis)an absolute plane can be described.

Creating this plane can be made dependant on conditions. To do so, activate the option Only create, if .

The figure below shows the plane according to the adjacent settings.

Black arrow = displacement vector

Black arrow = displacement vector

In the Fixed plane dialog, you can change the default name Absolute plane 1 under Last name.

[Note] Note

The changed name is only visible after an update.

The added absolute plane shows up in the history.

It can be removed with the Delete plane context menu command.

Via Properties... you can reopen the Fixed plane dialog.

Delete plane

Delete plane