powered by CADENAS

Manual

Manual

8.8.2.3.  Conditions

To reach an automatically working, correct course of the assembly configuration, the Conditions must be defined!

Otherwise unfitting configurations are possible due to improper row selection, as can be seen in the adjoining image.

Configuration- without conditions

Configuration- without conditions

Condition attributes window

Condition attributes window

HINGEDUMMY@L = WING1@L
HINGEDUMMY@L = WING2@L
HINGEDUMMY@D1 = BOLT@D
HINGEDUMMY@L = BOLT@L

Define the conditions using the above data.

[Note] Note

Refer to the conditions while defining - if possible - to the dummy starter-part.

Configuration - conditions

Configuration - conditions