Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Enter the appropriate variable of the table in which the number is located.
If a classification for eClass 4.0 was already conducted, for example, then this information can now be mapped to eClass 5.1.
Note | |
---|---|
Entries are only available in the pull-down menu if a mapping was conducted under Extras -> Class systems: map... (see Section 4.6.4.3.2, “ Class systems: map... ”). In the dialog box Set classification only classes are overtaken for: Classes with only suggestions and classes without assignments are not used when setting the classification. |
The classification can also be set via File.
The file must contain two attributes: class ID and NN (standard number). You can assign as many class IDs as you like for each standard number. |
|
Activate the checkbox and set the path to the file via the browse button .
Define Classification Number / Add classification number
If you don't want to loose old classification numbers, then better select Add classification number.
Note | |
---|---|
The automatism can also be used to fill your own classification. Example: Taking over the order number from a table row in order to build your own classification. More information for creating own classifications can be found under Section 4.14, “Apply own Class system ”. |