Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The "Grid" element is declared as "ELEMENT_" followed by a unique identification for that element.
[ELEMENT_grid1]
The following attributes are available:
Defines the space between the individual derivations in the y plane (see red marking in above image)
Defines the space between the individual derivations in the x plane (see red marking in above image)
Defines the unit in which the space is given. Currently only possible in PERCENT (based on box width).
If a parent is assigned, the grid aligns its breadth/height according to its parent. Without parent element, the grid takes up the entire space.
The following parent elements are possible:
box (see Section 4.11.3.5, “[ELEMENT_box] as wildcard element ”)
Constructs a wildcard element.
The value is for example parent = box1, if the [ELEMENTE_grid1] in the [ELEMENT_box1] is to be embedded. See example 2 below.
frame (see Section 4.11.3.9, “[ELEMENT_frame] Combine more elements in frame ”)
Via "ratio_title" beneath the title you can add the ration title.
Note | |
---|---|
In a separate block the properties for the ratio title must be defined. The block name must be set up as follows: ELEMENT_<Wert von "ratio_title">
|
So that the ratio title can be displayed, you must set "ratio_title_show" to "true".
If no box is being used as parent, the entire available space is used. The size of the grid CANNOT be changed in Edit mode. |
If a box is being used (see Section 4.11.3.5, “[ELEMENT_box] as wildcard element ”), it can be selected in Edit mode and the size maybe changed. |
[Template] name=grid_ohne_box unitbase=mm [Description] default=Grid without box german=Grid ohne Box english=Grid without box [ELEMENT_grid1] type=grid padding_x=10 padding_y=10 padding_unit=percent columns=2 rows=2 order=top,none,front,left
|
[Template] name=grid_mit_box unitbase=mm [Description] default=Grid with box german=Grid mit Box english=Grid with box [ELEMENT_box1] type=box align=center position_x=20 position_y=20 position_w=230 position_h=245 [ELEMENT_grid1] type=grid parent=box1 padding_x=10 padding_y=10 padding_unit=percent columns=2 rows=2 order=top,none,front,left
|