powered by CADENAS

Manual

Manual

4.9.21.  Release Notes tabbed page

How to set and edit Release Notes?

Section 5.10, “ Publish catalog ”In order to set new release notes (normally before publishing), do the following:

  1. On the left side in the index tree select the catalog.

    -> Now on the right side the Release Notes tabbed page is displayed.

  2. Click on the tab.

    -> The respective dialog box opens.

    If earlier entries exist, all these are displayed.

  3. Click on the button Add entry .

    -> A new section is opened.

    Enter the new release notes there.

In order to edit or delete entries, put the cursor into the desired field.

Then click on to edit or on to delete.

Where are the Release Notes displayed?

  1. The Release Notes are displayed in PARTdataManager.

    On the catalog directory click on the context menu command Release Notes....

  2. The Release Notes are displayed in PARTadmin.

    In the category Catalog update -> Online, on the catalog directory, click on the context menu command Release Notes....

Translate Release Notes

Once the catalog itself is selected on the left side in the tree, in the Edit project window, on the Translation tabbed page the single notes are listed.

Preview:

When you move the mouse over a line in the left column, a preview with the original terms appears.

Translate/edit:

  1. Select the line to edit.

  2. Right-click into the cell with the desired translation target language.

    -> The context menu opens.

    Click on Edit value.

  3. -> The Translation dialog box opens.

    On the left side you can select one of the already translated languages via tabbed page.

    On the right side the target language is displayed. Set the cursor into the desired text block and edit the content. Switch to the HTML view tabbed page - if needed.

  4. If you translate a target language, still without content, may be it is helpful to use the context menu commands Select All and Copy on the left side and to paste the content into the target language on the right side using the Paste command.

    Select All - Copy

    Select All - Copy

    Paste

    Paste

  5. Close the dialog box by clicking on OK.

Rights management:

If you use the SVN rights management, it is possible to only checkout the file releasenotes.xml for editing.

Information on translation in general is found under Section 4.8.2.1.13, “ Translation ”.