Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
If you used the Media editor for the creation of variables, then these are only available for the set Test project. But normally they should be available for the whole catalog. That means, the variable properties have to be inherited to the other directory levels up to the catalog level.
In PARTtemplateDesigner, in the settings dialog for Template, click on the button Open in PARTproject.
In PARTproject select the tabbed page Documents.
In the dialog area Derivation hierarchy, select the project (if not already selected), which you had chosen as Test project in the Media editor.
In the dialog
area Key select the Media variable to be inherited. In the
above exemplary figure this is "Headline_Merkmal
", which has
been needed for Alternative table header -> Class variable.
Compare "Table".
In the dialog area Derivation hierarchy, click on the icon Apply to the parent directory . Inherit the variable property step by step up to the catalog level.
In PARTdataManager, test, whether the variable value is correctly displayed at all projects.
Repeat the
procedure for all Media Variables needed on catalog level. Also for
"_Columns
" for
example, which is used for the table structure (compare Section 9.6.2, “Edit table
variables”).