Im PARTdesigner used variables
which, in turn, are generally components of formulae. The formulae of
complex designs are, in turn, very extensive so that syntax errors or
superfluous characters for instance may creep in. Such formulae can be
“cleaned up” using various optimization methods.
Note
Particularly in the case
of frequent mirroring and rotation of a part, it is advisable to use the Formula optimizer. Otherwise, terms would
be prolonged with every action and could thus reach the maximum permitted number
of characters of 256.