Frequently, individual part drawings
are combined in one DIN standard group, i.e. these drawings
feature similar or identical line styles and font types. The
File structure field contains the Clamp entry option so
that the same settings do not need to be made for each part in
a very large file structure for instance.
This means, that if you activate this
option, the various settings need to be made in one
file only and these are then automatically applied to the
remaining files in the directory.
This option can be activated via
context menu by clicking with the secondary
mouse button on a directory contained in the
File structure field.
Note
The directory icon of a clamped
directory is highlighted in red.
You can cancel the clamping
function again with the Remove pinning option in the context menu.
Note
After
you have selected a start directory, this directory is automatically
clamped!