powered by CADENAS

Manual

Manual

8.5.2.6.3.1. Value range columns

Value range columns: Certain assemblies have variables to which no fixed values are applied. The concerned columns (in the following example "POS", "NUT" and "F") are highlighted in yellow, respectively orange, as the case may be for UNIX systems, these are characterized in the title with the word Joker ( *). To enter a particular value for this column, click the corresponding field.

There are 3 kinds of value range columns:

  • Value range

  • Value ranges with images

  • Name of value

In the following image these are "POS", "NUT" and "F":

Value range - "NUT" without image

Value range - "NUT" without image

Value range Name of value with graphics Name of value

Value range

Value range

Name of valueValue ranges with images

Name of valueValue ranges with images

Name of value

Name of value

Enter the desired value in the default area.

To clarify the selection options in the domain columns, graphics may also be used.

Click the appropriate preview image.

Choose one of the default values.

--> Aside from the table entry, the display of the 3-D view changes as well.

You also have the option to display the graphic in the table's columns.

Value range - "NUT" with image

Value range - "NUT" with image

Show graphics in table