powered by CADENAS

Manual

Manual

14.2.2.2.2.  Scale and Paper formats

For the following views, the display can be exported with a sketch frame or with a sketch frame and integrated BOM-list.

  • 3 views + isometric drawing in frame (ANSI)

  • 3 views + isometric drawing in frame (DIN)

  • 3 views + isometric drawing in frame (JIS)

  • 6 views + isometric drawing in frame (JIS)

  • 3 views + bill of material in frame (ANSI)

  • 3 views + bill of material in frame (DIN)

[Note] Note

Depending on type the respective paper formats are displayed. On this see under Section 14.2.2.2.2.2, “Adjust paper format in 2D view”.

The following adjustments may be made:

See the following sections for more information.