powered by CADENAS

Manual

Manual

9.5.1.6.1.2. Context menu of the fields Condition 1 and Condition 2

In the fields Condition 1 and Condition 2 you cannot enter only manually but also set formula- and variable names via the appropriate context menu. The context menu provides extensive opportunities to define conditions. Via Functions , Operators , Logicand Brackets various formula names, including variables, can be combined arithmetically.

  1. Via Choose variable... open the Variable browser window, in whose field Parts the equation names (abbreviations) of all existing parts are to be listed.

    --> In theVariables of part field, all variables pertaining to the marked part are displayed.

  2. After confirming with OK the part and Name of variable are taken over, separated by an @ symbol, into the field Condition 1 and/or Condition 2 .

    --> A completed conditions shows up in the Configurator as subordinated entry (see fig.).

[Note] Note

The Delete of a Condition occurs without security question.