powered by CADENAS

Manual

Manual

6.9.3.2.5. Level 5

Coming from level 5, the following QA levels can be set:

Set QA status

1 - Not released yet

2 - Released for editing (by customer)

3 - In progress

6 - QA validation of group leader

In this stage, the Editor has the following possibilities:

  1. He sets the status back to 1, because relevant data is missing or incorrect.

  2. He sets the status back to 2, because he found additional deficiencies for example, or another editor takes over the project.

  3. He sets the status back to 3, because he found additional deficiencies for example, and wants to re-edit the project on his own.

  4. He sets the status up to 6, because the project passed his quality check.