powered by CADENAS

Manual

Manual

6.1. Which objectives are achieved with PARTproject QA?

The whole process of Catalog creation becomes transparent.

A release status of a catalog can only be reached if it runs through all of the steps up to the release status 8.

It is always apparent who has the working rights . Only one person may work on a project at one time.

More than one person may work within a catalog directory.

Corresponding symbols help get an overview to which QA-status a project/directory currently holds. From here, the respective responsibility is automatically reduced.

Further symbols make the processing status, in which the respective project/directory is currently situated, visible.

An analysis of processes can be carried out at any time - when and how long a catalog part was situated in which status level.

The control of QA State Generation and Live State Publication can be directly performed from PARTproject. Detailed Information on this is found under Section 6.14, “ Publish catalog ”.