Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
With the help of a small example the working when creating a new dimensioning shall be shown.
A horizontal dimensioning shall be created for a hole diameter.
In PARTdataManager, in the Part view, load the part to be dimensioned.
In PARTdataManager, open the dialog area Dimensions by clicking on the same-named command in the context menu of the toolbars.
-> The dialog is displayed as docking area. You can detach the area via drag and drop so that it is displayed as a single window.
Make sure that dimensionings are displayed in the 3D view.
Therefor, in the toolbar of the 3D view, click on the button Show dimensionings , if needed.
Make sure that the connection points are displayed in the 3D view.
Therefor, in the toolbar Montage, click on the button Show connection points.
Click on the button Create new dimension .
-> The respective dialog box opens.
In the list field, select the option HORIZONTAL and confirm with .
-> In the upper half of the dialog area Dimensions a new ID is automatically created.
-> In the lower half of the dialog area Dimensions all corresponding parameters are displayed.
Under Mandatory parameters -> Views select the desired 2D view(s), where the dimensioning has to be displayed.
Now determine the Start point of the dimensioning.
Click into the input field of Start point and enter the name of the connection point via Ctrl+V from the clipboard.
In the list field of Position, select the value BBOX (Bounding box) and under Offset (BBOX) enter the value 10.
-> As soon as all Mandatory parameters are set, the dimensioning is shown in the 3D view.
If needed, you can modify Optional parameters (e.g. Text) or set (e.g. Arrow size).
A complete summary of all PARTdesigner expressions can be found under Section 7.8, “Functions - PARTdesigner-Expressions ”.
The set dimensioning is also used for the 2D derivation.
When exporting to the CAD system the dimensioning is transferred as well.