Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
--> The dimension lines become visible at the mouse pointer. --> All dimension elements and the menu window Change parameter become visible. |
Define the Offset value (dimension to reference axis) and the Height (Type size) of dimension (see fig.).
Default is "{AUTOMATIC%0}" with curly braces.
"AUTOMATIC" takes the current value from the geometry. (Not recommended).
Define a static, dynamic or mixed static-dynamic Measure text.
Using %"number" you can define Decimal digits. (For example: A={A%2})
Note | |
---|---|
To satisfy high design demands, you can create external preview pictures and provide it as *.pra file for example. On this see Section 5.5.2, “*.pra files ”. Dynamic generation of the variables content in the measure text is only possible like described above! |
(In the above example "%0", so that the Measure text "8" without decimal places will be displayed)