Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Insert an existing sketch into the currently opened one, or replace the current one. These sketches may have been created either: |
Depending on the File type (*.dbs, *.dxf, etc.) that you select, a specific window opens (see Section 7.5.4.3.12.1, “*.dbs-, *.skt bzw. *.hsk files - "Insert sketch" window ” and the following ), in which you can make settings concerning the import of the sketch. |
See under Section 7.5.4.3.12.2, “Window „DXF Import“ ”. |
||
Those changes that have been made since opening the sketch are saved and the Sketcher is closed. If there is an Error in the sketch, is cannot be saved. An error message will be displayed (see figure). |
||
The changes that have been made since the opening of the sketch will not be saved. |