powered by CADENAS

Manual

Manual

6.9.3.2.3. Level 3

Coming from level 3, the following QA levels can be set:

Set QA status

1 - Not released yet

2 - Released for editing (by customer)

4 - Validated from editor

In this stage, the Editor has the following possibilities:

  1. He sets the status back to 1, because relevant data is missing or incorrect.

  2. He sets the status back to 2, because another editor takes over the project.

  3. He sets the status up to 4, because the project is finished and well verified from his point of view.