Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The following overview on optional parameters applies for all types of dimensioning and annotation:
Text can be created in different ways:
{AUTOMATIC}: An automatically generated value of dimensioning (default)
{AUTOMATIC}
Delete the expression "{AUTOMATIC}" and enter the desired text.
Any text combined with an automatically generated value of dimensioning
The degree symbol shall be displayed in addition to the value of dimensioning.
{AUTOMATIC} °
Any PARTdesigner expression can be used.
E.g. {partname@variable}: Part name with declaration of variable
This dimensioning has the length {RZ500@D}
If the automatic calculation of the numeric value does not result in an adequate rounding (9.99999), you can choose another way of calculation with PARTdesigner expressions (see Section 7.5.4.5.3, “Functions ”).
You can also convert from inch to mm and display the unit in addition.
If there is no statement, then 3.5 is set by default. Unit is according to the drawing unit.
Alternatively you can use PARTdesigner Expressions.
15*RZ500@D/20
IF SHORTVIEW@HUB2D=0 THEN AUTOMATIC ELSE AUTOMATIC+HUB-SHORTVIEW@HUB2D ENDIF
IF SHORTVIEW@HUB2D=0 THEN AUTOMATIC ELSE H2 ENDIF
0.5
The relation between arrow size and font size is fixed.
The value of Arrow size is a factor. 0.5 for example halves the arrow size in relation to the default size.
As an alternative you can use PARTdesigner Expressions.
15*RZ500@D/20
For new created dimensionings as of version 9.08 SP0 this parameter should be used. Older versions will not interpret it. Without special declaration the versions from 9.05 to 9.07 SP0 will display normal arrow size. Versions <= 9.04 will display smaller arrows
All statements concern the automatic dimensioning described here, but not the interactive dimensioning via toolbar.
The value specifies how accurate a numerical value on the dimensioning arrow has to be.