Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In order to make catalogs available for download from the Internet, for example, these can be cipped, in other words reduced in data size. The conditions needed to be fulfilled can be entered in the CIP catalog window.
On the left side of the window you can see a Catalogs column. There you will find all previously cipped catalogs.
All checked directories are cipped by clicking on the button.
You have different selection possibilities available to you in the list field.
Classifications may also be cipped.
When cipping class systems, the settings in Project selection are insignificant.
In this
case, the CIP catalog
dialog should be opened via the Extras menu and the entry should be
added manually in the Catalogs area
on the left. In the Classification
filed, the name of the classification must be entered exactly the
same as in the classsystem.cfg
classification file (in other words the terms that is located in
between brackets). Please make sure that upper and lower case
letters are correct.
As with catalogs, the full-textual search index may be created. To do so, activate the option Create search index.
For this selection only the indicated files will be transferred to the cip file.
The files are specified in the Additional directories field (see further below).
The spelling entered here will later be displayed during the installation in PARTadmin or during installation of the DVD.
Note | |
---|---|
If you do not enter a description, then the description given under Edit project -> General1 tabbed page -> Catalog name, or Name of installation will be used. The entry on the CIP catalog page has precedence.[15]
|
Enter the version of the PARTsolutions installation here in which the *.cip file should later be opened. If your directory contains parts of a newer version, these must then be adjusted.
Directory: the directory/catalog to be cipped (marked in directory tree)
License file: So that the project files belonging to a catalog cannot later be opened and exported in the PARTdataManager by unauthorized persons, each individual project is linked to a license ( for example, CNS2009*Folder1*READ or CNS2009*Folder1*EXPORT). All licenses that correspond to a catalog are stored in the so-called license file (ending *.cnsldb). This *.cnsldb - you can request one from CADENAS - should then be entered into this field.
Catalog license: In this field the basic license (for ex. CNS2009*Folder1) should be entered. You receive the basic or catalog license along with the *.cnsldb file.
If the *.cip file to be created is to contain directories or files enter them here.
Additional directories may contain individual help files for example, which you have applied within the Edit project menu -> Catalog help tab. Input via $CADENAS...\...\....
See also under Content -> list selection field Files.
Catalog is free (No check for CNS2000*MAINTENANCE) : For licensed catalogs, the so-called maintenance license is requested during the uncipping. If you do not have one, the catalog cannot be uncipped.
The encryption ensures against manipulation. The file contains a license key, for example.
Automatically adding external files
These may be located anywhere under $CADENAS_DATA (the respective linking is located in the project file).
If you select this option, the index for the Full-text search will be created.
If you also want to create the GeoIndex (fingerprints for the geometric search), enter values into the fields Percentage and Absolute fraction. The default entry "-1" means that no GeoIndex will be set.
Sample calculation 1: 10 rows, Percentual fraction: 10, Absolute fraction: 3 -> 3 rows are created
Sample calculation 2: 10 rows, Percentual fraction: 20, Absolute fraction: 1 -> 2 rows are created
Thus the larger of the two values is always taken. The time for generation and the memory space for the fingerprints is approximately proportionate to the number of rows.
Tabbed page Test catalog (see ???)
Note | |
---|---|
Before you can begin to make settings in the individual fields, the option Perform tests must first be activated. |