Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Via text attributes it is possible to pin on additional information (e.g. special characteristics of surface) at the model.
In order to create a CAD text attribute insert the desired text in the CAD text attribute on face field.
Surface CAD text attributes are only processed by ProE at the moment.[37]
In V9 now it is possible to use HTML attributes with surface attributes. At the moment[38] these are only displayed in PARTsolutions. In order to create a text attribute insert the desired text into the HTML text attribute on face field.
Note | |
---|---|
The usage of pictures or links is possible in a restricted manner.[39] <img src=“$CADENAS_DATA/pics/mypic.jpg“>
|
For the 3D view, you can define clickable text fields to part faces and connect them to variables.
Variable description text, color of the variable table column and the actual value of the variables in the 3-D view are automatically transferred to the displayed labeling field (see following figure).
On the Face attributes page, enter the desired text into the HTML text attribute on face field.
Define the connected variable.
This enables you to differentiate what is to be shown in the single part/configuration mode and what is to be shown in the Assembly-Table mode.
On the one hand they may be different variables, but on the other hand they may hide the label: If you only assign one variable for the single part but not for the Assembly-Table, then the entire label will be invisible in the Assembly-Table mode.