Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
This element indicates whether and which paper formats are to be made available for this view.
This element is optional and should only be used if different paper formats are truly available.
In the 2D view dialog window, in the Paper formats list field, select the desired format.
The following describes how the different paper formats are declared:
Via [ELEMENT_frame] in the template file *.dw the default frame is defined.
[ELEMENT_frame] type=frame dxf=default.dxf
Via [Formats], also in the template file, the additional paper formats (frames) are defined.
The input under [Formats] refers to configuration files.
Display name = path to *.cfg configuration file.
[Formats] A0=defaultA0.cfg A1=defaultA1.cfg etc.
The configuration file under [ELEMENT_frame] refers to another dxf file (paper format).
[ELEMENT_frame] type=frame dxf=defaultA0.dxf
In the
*.cfg
configuration file, all elements
of the sketch view (*.dw) are indicated with their valid geometries
relevant for the paper format (height, width, etc.), so that these can be
displayed in the new paper format as well.
The following figure shows the storage directory with standard 2-D derivations, translation files, configuration files and DXF files.