Click on cut off point. -->
Excess line area will be removed.
Trim elements to each other:
Stub and/or trim two lines onto a
corner.
Click on first
element to be trimmed.
Click on second
element to be trimmed.
Click on
intersection or "cut-off corner".
Cut element between 2 elements:
Remove line area between two points.
Click on
element to be split.
Click on
starting point of the area to be removed.
Click on
endpoint
Trim length of line:
Change line length.
Click on line at fixed end.
Click on intersection or "cut-off
corner".
Set exact new length of line in the
Change parameter window.
Radius with 2 elements:
Chamfer lines that do not
intersect.
Click on first
line and/or circle..
Click on the
second line and/or circle.
Position radius
with cursor.
Set exact
radius in the Change parameter window.
Chamfer at 2 lines defined by angle at distance from intersection:
Chamfer between 2 lines,
"adjustable" via the angle to the first selected line and the
distance of the chamfer to the (imaginary) intersection of both
lines
Click on first line.
Click on second line.
Set exact
distance (1) and angle
(2) in the
Change parameter window.
Chamfer at 2 lines defined by angle and chamfer length:
Chamfer between 2 lines,
"adjustable" via the angle to the first selected line and the
length (chamfer).
Click on first line.
Click on second line.
Set chamfer
length (1) and angle
in the Change parameter window.
Chamfer at 2 lines defined by angle and chamfer height:
Chamfer between 2 lines,
"adjustable" via the angle to the first selected line and the
indent length (distance chamfer/intersection).
Click on first line.
Click on second line.
Set indent
length (1) and angle
(2) in the
Change parameter window.
Chamfer centered at 2 lines defined by distance to intersection:
45° chamfer between 2 lines,
"adjustable" via the length of the distance of the chamfer to the
(imaginary) intersection of both lines..
Click on first line.
Click on second line.
Apply exact
length (1) in window
Change parameter.
Chamfer centered at 2 lines defined by chamfer length:
45° chamfer between 2 lines,
"adjustable" via the length of the chamfer.
Click on first line.
Click on second line.
Apply exact
length (1) in window
Change parameter.
Chamfer centered at 2 lines defined by distance to intersection:
45° chamfer between 2 lines,
"adjustable" via the length of the cut line area.
Click on first line.
Click on second line.
Apply exact
length (1) in window
Change parameter.