Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Last name: Per default "Base extrude xy" shows up. The numbers go up consecutively with each new extrusion.
You may change the name. However, use only ANSI characters (in other words: a-z, A-Z, 0-9 and spaces).
In the Length field you can set the measurement of the stretch of the 2-D object.
Against surface normal extruding means pulling into opposite sides. |
Both directions completes the extrusion along and against the plane normal. |
|
|
Draft : In order to create a draft from a 2-D sketch, enter the respective angle measurements into the draft field. |
You can connect a Condition to an extrusion as well. Possible characters are &, |, !=, =, >, <, >= and <=. |
Example: The sketch should only be extruded if for variable H (height) ea value larger than 10 has been set. |
Construction steps (features) which, based on their condition are excluded, will be deactivated in the history and identified by a symbol.