Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
Sectional cuts are marked by hatches in the 2D preview. How these are changed for each part of an assembly can be configured via the following settings:
Possible hatch angles: 0.00,10.00,20.00,30.00
In the example, the first hatch angle is therefore 45° (+0°), the second 35° (-10°), the third 55° (+20°) and the fourth 25° (-30°).