Translation: Distance between two connection points
(via value or variables). In the figure on the right
side the profile shifts (later on in the CAD-system) in
the defined distance between the connection points 1 and
2.
Rotation: The part rotates around a connection point (via
angle or variables).
Tilt: ...allows inclination related to a
connection point.
Swivel: ...enables turning in an inclined
position.
Option free: Allows to rotate assembly elements (exported from
PARTdataManager into the CAD-system)
free around the rotation-, translation-, swivel- or
tilt-axis.
If the
option Free is
activated, a minimum and maximum position can be set for Translation and Rotation.
Note
The element start position in the
CAD-System can be defined via the fields Rotation and/or
Translation.
Free rotation or translation is only
possible if in the CADENAS PARTsolutions interface the
automatic link
function to the CAD-system was activated!
Reverse direction:
The part is rotated 180
degrees at the connection point concerning
the Z axis.