Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Basically you can activate this function.
However the following warning notice always shows up:
If there are problems with the building of an assembly, check if it is possible to avoid the error by deactivating the check box.
Concerns assembly configuration and templates. With the Assembly-Table-Project there is no access to the single parts, since these are controlled by the table.
After activation, the corresponding context menu item is grayed out.
Append free connection points automatically
This feature does not concern the Assembly-Table-Project since clarity is warranted in the steering table anyway. However the stencil, which is the basis for the Assembly-Table-Project, should have been created in the below mentioned way.
Assembly-configuration and template
Prerequisite for the use of the option: Conditions ensure that there is only 1 row available per connection part.
There is no damage, if the option is activated, even though the terms are not met; but an automatic buildup is then impossible!
Initial situation: A specific set-up of the configuration (see figure).
In the menu window do not activate any of the checkboxes.
The option especially, may not be activated!
Equally, the magic stick (build assemblies automatically) may not be activated!
Delete all parts, except for the starting part! (This can also be a dummy.)
Save the template in this state!
Is currently only supported by Inventor. The interpretation can be found in CAD.
extended attributes -> PSOL_MULTISOLIDPART 0: Zu einem Teil verschmelzen 1: Als Baugruppe exportieren z.B. EXTATTRVAL{ NAME{ "PSOL_MULTISOLIDPART" } VALUE{ 0 } }
Invalidate changed tables even if the chosen line is still available.
Export single part assemblies as single parts
In case the assembly is comprised solely of one part, it will be exported as a single part.