powered by CADENAS

Search PDF Catalogs

  •  
  •  

PDF Catalogs

  • Created April 27, 2015 by Airtècnics ., 0 comments, 1,397 views, 1 like, Category: Air Condition
    TOTAL ULTIMATE CONTROL FOR AIR CURTAINS MANAGEMENT: The future is here with the new generation Clever control. Maximum control, maximum energy saving. Clever automatically adapts the functioning of the air curtain to the entrance conditions in order to keep the comfort saving energy. Depending on door state, how often the door is open/closed, internal/outside temperature or discharge temperature, Clever optimizes the ventilation and heating to make an efficient barrier for an optimal climate separation. Manually or automatic functioning with many diffe..
  • Created April 27, 2015 by Airtècnics ., 0 comments, 976 views, 0 likes, Category: Air Condition
    Aware of the importance that the visual impact has in today’s society, Airtècnics have managed to combine to perfection them highest technology with the more exclusive beauty. Visit our webpage: www.airtecnics.com / www.dooraircurtain.com
  • Created April 27, 2015 by Airtècnics ., 0 comments, 1,248 views, 0 likes, Category: Air Condition
    Airtècnics air curtains are the ideal solution to control the indoor climate in commercial or industrial premises that need to keep their doors open.Air curtains create an invisible barrier that efficiently divides the internal atmosphere from the external one. They substantially reduce energy losses through the door, up to 80% while increasing employees and clients comfort. Visit our webpage: www.airtecnics.com / www.dooraircurtain.com
  • Created April 27, 2015 by Airtècnics ., 0 comments, 1,251 views, 0 likes, Category: Air Condition
    Air Curtains for revolving doors: The design of buildings with revolving doors that integrate with the environment is a common solution when the entrance has adverse conditions with high pressure differences, temperature differences or strong wind.To avoid the loss of energy produced with revolving doors and maintain a clean and healthy atmosphere, and air curtain must be installed. Visit our webpage: http://www.airtecnics.com / http://www.dooraircurtain.com
  • Created April 27, 2015 by Airtècnics ., 0 comments, 853 views, 0 likes, Category: Air Condition
    The new Airtècnics Heat Pump Air curtains are absolutely efficient reducing the heating cost and CO2 emissions up to 70%. - Very high energy efficency ratings to save big amounts of money on your energy bill.- Short Payback Period thanks to very high livel of energy saving.- Heating and cooling included in the same system (reverse cycle).- Environmentally Friendly as uses such low amounts of energy. Visit our webpage: http://www.airtecnics.com / http://www.dooraircurtain.com
  • Created April 27, 2015 by Airtècnics ., 0 comments, 905 views, 0 likes, Category: Air Condition
    A good way to integrate an air curtain in a premise, whether commercial or industrial, is by using recessed air curtains. This is possible provided that the premise has any element at the entrance that makes it possible recessed installation, as false ceiling, lateral columns or a bulkhead above the door. In Airtècnics we place a special importance to this type of air curtain and we already have 5 different models that adapt to any kind of door and needs. From resessed air curtains with visible surface or visible inlet grille, to air curtains inst..
  • Created April 27, 2015 by Airtècnics ., 0 comments, 1,532 views, 0 likes, Category: Air Condition
    Airtècnics air curtains create a high speed air flow acting as an invisible air barrier over the doorways. Its use can effectively separate the inside from the outside environment without limiting the access of people or vehicles. Visit our webpage: www.airtecnics.com / www.dooraircurtain.com
  • Created April 27, 2015 by Airtècnics ., 0 comments, 1,316 views, 1 like, Category: Air Condition
    Full range catalogue of Airtecnics air curtains 2015. New models: Maxwell air curtain, Recessed Dam air curtain, Recessed Compact air curtain and some heat pump air curtains.
  • Created July 26, 2013 by CADENAS Person, 0 comments, 1,043 views, 0 likes, Category: Air Condition
    Kühlkonzepte 19"-Lüftereinschübe Filterlüfter Kühlgeräte und Luft/Luft-Wärmetauscher Zubehör Heizungen
  • Created July 26, 2013 by CADENAS Person, 0 comments, 1,877 views, 0 likes, Category: Air Condition
    19"-Lüfter Filterlüfter Zubehör Luft/Wasser-Wärmetauscher