The following
table contains some possible error messages which may appear.
If you wish to
receive an error report, use the parameter -logfile during
launch.
Error
message
Description
No licence
available for
CNS2005*ADDONS*CLASSIMPORTER
You are
missing a license for the Classimporter.
Error moving directory: directory
name
If a directory
cannot be moved/copied from a temporary directory into a release
directory.
Error moving file: file
name
If a file
cannot be moved/copied from a temporary directory into a release
directory. Possible reasons: No write access in target directory;
hard drive or network problems.
Error reading file: file
name
The file could
not be imported. Either because it is not available or because a
read error occurred. (Hard drive or network
problems).
Error writing
file: file name
A file could
not be created. Possible reasons: No write access in target
directory; hard drive or network problems.
Cannot create directory: directory
name
A directory
could not be created. Possible reasons: No write access in target
directory; hard drive or network problems.
File not found: file
name
A transfer
file (TXT file from the SAP interface) was not
found.
Attribute definition file: file is
empty
The file
attributedef.txt is
empty. (A TXT file must contain at least one line: the line with
the column names of the TXT file)
Column not found: column name
In File:
file name
A column is missing from a transfer
file (from the SAP interface)
Attribute definition file: Unknown
attribute type
The attribute
type for the attribute in the attributedef.txt file
must either be called NUMBER or STRING.
Attribute definition file: Double
entry for attribute "attribute name"
Error in file
attributedef.txt. Two
attributes in a class have the same number.
Added attributes to class "class
name". But the class is not part of the class
structure
In attributedata.txt file
an attribute is assigned to a class. A class with this name
however does not exist in the class structure.
Attribute without Name defined for
class "class name"
An attribute
in the attributedata.txt file
does not have a name.
Error in value range (class "class
name"; attr "attribute name") max value has to be larger then min
value
Error in a
value range. The upper limit must always be larger than the lower
limit.
Attribute "attribute name" not found
in definition file
In the file
attributedata.txt a
value is always assigned to an attribute. This attribute is not
defined in attributedef.txt
however.
No ERP_PDM_NUMBER found for material
number
A material
number which is used in the file attributedata.txt could
not be found in the database. This means it is missing in the file
erpdata.txt.
prjtab import: Class "class name" not
found
In the file
prjtable.txt a
class is assigned a value. However, a class with this name does
not exist in the class structure.
Cannot create object
cnstools.psolgeomdatabase
The file
proxygeomdatabase.dll was not found i the directory ../partsolutions/software/libs/x86/com.
Can't create cluster
file
An error
occurred while creating a cluster file for the geometrical
search.
Error creating geometric sample for
STL file
An error occurred while creating a
comparison value for the geometrical search.
No POODIR
defined in classimport.cfg
No pool
directory was defined in the file classimport.cfg. The
pool directory must be defined under the key
NATIVEPOOLDIR.
Error in ODBC-Driver …
SQL: SQL
allocation
Error while
carrying out an SQL allocation.
Warning: Attribute name adapted (from
Name to Name) (class: "class name")
The name of
an attribute does not correspond with the PARTsolutions
conventions. It was thus accordingly adjusted.