![]() |
When using the
command Copy dataset you can transfer values from one
dataset (project line) to another dataset (project line). In order to insert
the data, in the dialog box Edit dataset, use the
button .
The following example shows how to use the function:
In the table, select a dataset (a project line), whose values you want to copy.
in the
ClassificationToolbar, click on the button
Copy dataset .
In the table, select that line where you want to paste the copied values.
In the
ClassificationToolbar, click on the button
Edit dataset .
-> The dialog box Edit dataset opens.
Now you can manually edit single values.
However, you can also directly paste the copied values from the clipboard.
Therefor click
on the button . You can paste only the Table data, only the ERP data or both data types.
In the example in hand only ERP data is inserted.
Result: Now the table data are identical at matnr4 and matnr18, but the material differs.