![]() |
3.1.6.4.4.
Variables search
3.1.6.4.4.2.
Variables search: Call
from dialog area "Suggestions"
|
|
---|---|
Prev | Next |
In order to perform a Variables search proceed as follows:
On the tabbed page Part selection -> subpage Structure -> Catalogs, limit the search on Standards -> ISO -> Bolts
-> In the docking window Suggestions the common variables of the selected directory level are displayed. Here, exemplarily "Variables for Bolts".
-> A selection dialog with the options New search or More precise (AND) opens.
-> The dialog box Variables search opens. The input field of the variable D is already selected.
Enter the desired value for D, furthermore the desired value for L. Leave the mathematical operator on equals (=).
-> The
respective rows are marked with an icon .
Alternatively the dialog box Variables search can be opened by clicking
on the link or under
Add search function on the button Variables search.
-> Now the method is displayed with the currently chosen parameters.
You can use
the variable search as only method or in combination with others. Not
desired methods can either be deactivated (clear checkbox) or be deleted
). In this example we will use the variable search
as only search method. Disable the Full-text search (delete is not possible at
full-text search).
Click on the
button Start search.
-> The
search results are listed on the Search results tabbed page. At each hit,
when you click on the plus sign below the part family the single parts are
listed. The following figure shows 1 line, which exactly meets the query
(D equals 30 and L equals 100)
When moving the mouse over a result line, then different buttons are displayed.
Top left at
the icon Search filter on/off you can recognize, that the characteristics have
been filtered. If you want to see all characteristics, then click on the
icon.